Issue:
Setting up jog function similar to the other Altivar Drives
Product line:
Altivar 630, Altivar 650, Altivar 660
Environment:
all
Cause:
n/a
Resolution:
A Jog function is not available on the Altivar 600 series drives. It is available on the 900 series drive.
If the VFD is set for 3-wire control, then change to the 900 series.
If the VFD is set for 2-wire control, then the Preset Speeds function may be acceptable. Note that the Preset speed used for the jog speed will not run the motor at less than the Low Speed setting.
Setting up jog function similar to the other Altivar Drives
Product line:
Altivar 630, Altivar 650, Altivar 660
Environment:
all
Cause:
n/a
Resolution:
A Jog function is not available on the Altivar 600 series drives. It is available on the 900 series drive.
If the VFD is set for 3-wire control, then change to the 900 series.
If the VFD is set for 2-wire control, then the Preset Speeds function may be acceptable. Note that the Preset speed used for the jog speed will not run the motor at less than the Low Speed setting.
Released for:Schneider Electric Saudi Arabia