{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to disable one of the M580 MAC address?
Issue:
Why does the M580 have multiple MAC addresses and how can I turn them off or remove the additional MAC address?

Product Line:
M580

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
M580 has an embedded switch whose ports have different MAC addresses.
Per design, there is no way to turn off the MAC of the M580 ports. Only 1 MAC address which is the first port (service port) MAC is laser hatched because this represents the MAC address of the product at the same time. The other MAC addresses are +1 and +2

Schneider Electric Saudi Arabia