{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there instructions showing the proper way to install the gasket material of a Vertical Exhaust Duct Kit?
Issue:
Pieces of the gaskets are loose or falling off.

Product Line:
Vertical Exhaust Duct Kits

Environment:
All versions and serial ranges

Cause:
If the gasket is not installed properly it will not adhere.

Resolution:
The installation manual has been updated with instructions for correctly installing gaskets to the top of the duct, and NetShelter door frame.
You can also find a gasket installation video from Trim-Lok at this link: https://www.trimlok.com/rsinstall
There is also a document attached below that explains correct installation of the gasket.

Spare Gaskets:
We may have 8.4m pieces of the gasket used on the door frame in stock as spare part 0J-827-0292A.
We do not have spares for the gasket used atop the duct. It's Trim-Lok pn: X-1153HT-SINGLE. (HT, Black, single) Trim-Lok sells this by the 1,000 foot box.
https://www.trimlok.com/rubber-extrusion/epdm-seal/d-profile/1153-series

Schneider Electric Saudi Arabia

Attachment(s)
20170425 VED Kit Gasket Installation Instructions rev1.pdf [31.79 KB]