{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can other manufacturer's cabinets be installed in the HyperPod?
Issue:
Does HyperPod support other cabinet manufacturer's, or just APC NetShelter?

Product Line:
HyperPod

Environment:
All versions and serial ranges

Cause:
Customers may want to install a 3rd party cabinet into the HyperPod.

Resolution:
Yes, 3rd party cabinets can be installed in the HyperPod easily. Height differences are no problem with the adjustable brush strips that mate with the cabinet roof.

Schneider Electric Saudi Arabia