Search FAQs
Where can I get the cable pin-outs for the Modbus TCP connector for the Altivar Process Drive?
Issue:
Cable pin-outs for the Embedded Modbus Ethernet connector for the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Needs to know required cable connection pinouts
Resolution:
See attachment
Cable pin-outs for the Embedded Modbus Ethernet connector for the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Needs to know required cable connection pinouts
Resolution:
See attachment
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: