Issue
How to optimize Unity Pro Performance while working with LL984 Upgraded Projects Product Line Unity Environment Windows 10 Resolution This Tip is applicable to Unity Pro Versions V5.1 through V8.0. There are several things that a user can do to optimize the performance of Unity Pro while working with projects that are upgraded from Legacy 984LL Software.
In addition to the Project Setting Upload Information management, it is highly recommended that the Project Settings for Build are set.
|
Released for:Schneider Electric Saudi Arabia