{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the blinking COM status led mean on the ATV630 and ATV930 Process drives?

Issue:
ATV630 and ATV930 Process drives with blinking COM status led.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Com's status LED will blink when they connect the remote HMI display to the modbus port.

Resolution:
LED will flash when the fieldbus is active and communicating.

Schneider Electric Saudi Arabia