{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the various holes on the frame and roof of a NetShelter cabinet used for?
Issue:
Customers may ask what these various holes are used for.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges

Cause:
There are many holes on the outside of a NetShelter cabinet.

Resolution:
See attached file.

Schneider Electric Saudi Arabia

Attachment(s)
20170518 Various Mounting Holes Function Rev1.pdf [129.75 KB]