{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up fault reset over the network with the ATV630 drives embedded Ethernet in I/O profile mode?
Issue:
ATV630 drives embedded Ethernet in I/O profile mode set up fault reset over network.

Product Line:
ATV630 or ATV930 in I/O Profile mode only

Environment:
All

Cause:
Wants to reset the faults over Ethernet using Bit 1 of the command word CMD.

Resolution:
With Profile set to I/O the assignment for fault reset will be C501 as fault reset being Bit 1 of the CMD with embedded Ethernet and I/O profile.
C501 means Bit 1 of the CMD 8501 will allow the faults to be reset over the embedded Ethernet network.

Schneider Electric Saudi Arabia