Issue:
Connect the VW3A3616 Ethernet card to the ATV320 compact version.
Product Line:
ATV320 with C suffix only
Environment:
All
Cause:
There is not a slot for the Ethernet card card to fit the ATV320 with C suffix.
Resolution:
The VW3A3616 card will not fit directly into the ATV320........ C or compact version drive without the VW3A3600 add on option.
The VW3A3616 card will fit directly into the ATV320 ....... B or Book self version without the need of the VW3A3600 add on option.
Connect the VW3A3616 Ethernet card to the ATV320 compact version.
Product Line:
ATV320 with C suffix only
Environment:
All
Cause:
There is not a slot for the Ethernet card card to fit the ATV320 with C suffix.
Resolution:
The VW3A3616 card will not fit directly into the ATV320........ C or compact version drive without the VW3A3600 add on option.
The VW3A3616 card will fit directly into the ATV320 ....... B or Book self version without the need of the VW3A3600 add on option.
Released for:Schneider Electric Saudi Arabia