{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
DUP2 Does Schneider Electric offer the Berger Lahr EXRDM3913/50NEA motor or a suitable replacement?
No, the Berger Lahr EXRDM3913/50NEA motor with ID number 52951045500 is a special customized version for the company W&H.
This type is proprietary and is reserved for the company W & H and can not be purchased from Schneider Electric.
The customer must contact the OEM machine builder Windmuller & Holscher for a spare EXRDM3913/50NEA motor with ID number 52951045500.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: