{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SoMachine V4 showing "DPI settings not supported"
Issue:
SoMachine V4 showing "DPI settings not supported"

Product Line:
SoMachine V4.2, V4.3

Resolution:
The DPI is changed in the Windows settings. In Windows 10 that is available under Settings / Display
Windows DPI settings should be set to 100%
The computer needs to be rebooted for SoMachine to recognize the new setting.
Starting with Machine Expert 1.1 this problem should not appear anymore.
Note: SoMachine is an older Software and does not support 4k resolution.

Schneider Electric Saudi Arabia