{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the new features in SoMachine Basic v1.3 SP1?

The new features in SoMachine Basic v1.3 SP1 are:

New controller starting mode: "Unconditional start in Run" (allows controller to start in Run after applying power without battery charged or present)
Memory Consumption View
Trace
Report (Print): cover page, project info, symbol list, cross-ref, user program (IL+LD)
Symbolization of function block members
Possibility to remove temporary project protection

Schneider Electric Saudi Arabia