{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME@local host is not detected when Detect Event Sources is selected in the ENM Configuration after ENM 8.3.x is installed.
Issue:
PME@local host is not detected when Detect Event Sources is selected in the ENM Configuration
after ENM 8.3.x is installed, it should be showing as the screen shot below



Product Line:
Event Notification Module (ENM) 8.3
Power Monitoring Expert (PME) 8.x

Environment:
Windows Server

Cause:
Unable to configure ENM since is not detecting PME@localhost.

Resolution:
Need to make sure ENM is licensed before trying to configure ENM.
Verify that ENM is activated and listed under Floating License Manager.
For instruction on how to license ENM, see the  licensing guide under the FAQ article: FA225923.



Schneider Electric Saudi Arabia