{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam and ACE850. What are the Sepam compatible with ACE850 and IEC 61550 Protocole ?
Sepam and ACE850. What are the Sepam compatible with ACE850 and IEC 61550 Protocole ?

The Sepam that are compatible with ACE850 Accessory are :

Sepam 40 with Version >= V700 and S/N >= 09500001
Sepam 60 with Version Base >= V7.20 and Appli >= V7.10
Sepam 80 with Version >= V6.01 and Appli >= V6.02

IEDL3

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.