{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Installation of LC1F800 turned 90 deg. from standard (vertical) position.

Side turning 90 deg. from standard position (main pole connection to the left and right) is possible for LC1F800.

However, the position for aux. contacts on LC1F800 has to be up - see Attachment1.
The installation with position for aux. contacts on LC1F800 down is not allowed.

Schneider Electric Saudi Arabia

Attachment(s)

Attachment1.pdfAttachment1.pdf [171.86 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: