Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
On a ATV320 drive, what would cause register 5202, reading logic input status LI6, not to turn on?
Issue:
Register 5202, reading logic input status LI6, is not to turning on when the input is energized.

Product Line:
ATV320 drive

Environment:
All 

Cause:
LI6 status is not showing up on register 5202 logic input status. 

Resolution:
Reading address 5202 over Canopen or modbus and bit 5 for LI6 is not turning on. 

When inputs are wired for SOURCE;
Verify the SW1 switch is in SOURCE position.
Verify the input by measuring LI6 - COM for 24Vdc.  
Verify the SW2 switch is in DI6 position.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: