{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the Profibus Fieldbus Option Module for the Altivar Process Drive?
Issue:
Part number of Profibus Fieldbus Option Module for the Altivar Process Drive.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
VW3A3607 - PROFIBUS DP Module for Altivar Process Drive with a sub-D 9 female connector

Schneider Electric Saudi Arabia