{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the default serial port settings in PM2225 meter ?

The meter is factory-configured with the following default serial communications
settings:

• Protocol = Modbus RTU
• Address = 1
• Baud rate = 19200
• Parity = Even

You can use a communications converter (USB to RS-485 or RS-232 to RS-485)
device to connect to the meter.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: