{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Data Center Expert | How can I export data?

Issue:
Process for exporting data from StruxureWare Data Center Expert.

Product Line:
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)

Environment:
StruxureWare Data Center Expert (All Versions)

Resolution:

Information can be exported from Data Center Expert using the DCE Desktop Client or SOAP Web Services.

Exporting Data from the DCE Desktop Client

NOTE: Certain panes within the DCE Desktop Client have an export option.

An example of how to export all devices from the DCE Desktop Client:

1) Log into the DCE Desktop Client.

2) Open the Monitoring perspective.

3) Within the Device Group pane, click on All Devices.
NOTE: You can select a different group to export just those devices.
NOTE: You can search for devices using the search bar within the Device View pane to filter what devices to export.

4) In the upper-right corner of the device view pane, select the folder with the green arrow on it.
NOTE: Selecting the drop down will allow for export as a CSV or TXT file.
NOTE: Only the columns that are currently being displayed will be exported.

5) Save the file and open in a program that can open the type of file you chose to save.




Exporting Data Using SOAP Web Services

For information on pulling data from DCE using web services, visit DCIM Support.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: