{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I setup an ATV212 Drive to start and stop from face display and speed up using an external potentiometer?

Article available in these languages: Spanish

Issue:
ATV212 configuration to start and stop from face display and speed up using an external potentiometer?

Product Line:
Altivar 212

Environment:
All

Cause:
Wiring and programming

Resolution:
Wiring for potentiometer:
PP for +10VDC
VIB for signal.
CC for common connection

Programming:
Mode and arrow under AUF.
Set CNOD to 1 for main front display start and stop.
Set FNOD to 2 for 0-10VDC from VIB and CC.

Schneider Electric Saudi Arabia