{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can we use BMENOP0300 with an M340 PLC?
Issue:
I need to have IEC 61850 communications. Can we use BMENOP0300 with an M340 PLC?

Product Line:
M340

Environment:
EcoStruxure Control Expert

Resolution:
No. BMENOP0300 is not supported by the M340, it works with M580 ePAC only.
It requires the use of the Ethernet backplane for communication.

Schneider Electric Saudi Arabia