Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Which function can we do with the ZBRT2 wireless button ?
This product is done to do only one function set-reset, that means the output of the receiver will be active when the operator will push the button and inactive when he will release it.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: