Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set TEsysT thermal protection for start-delta start?

Article available in these languages: Spanish

When TesyT is configured to 2-step operating mode (2-step 2wire or 2-step 3wire), this operating mode can be used for

  • Star-delta start or
  • Starting using starting reactors or
  • Starting using autotransformer

2-step operating mode means that step1 is temporary (starting) and step 2 is final step (running)

Please note that if TesysT is connected inside motor delta (wiring diagram shown in the manual) and you use 2-step operating mode you have to enable “motor star-delta” as shown on picture 1


picture 1
Picture 1 - Selection for star delta start


With this setting, the current flown via current transformer is sqrt(3) times lower in step 2 (delta), but TEsyst will recalculate and show always line current.
So FLC current must be set to line current (not for the current inside motor delta), this value can be copied from motor plate for delta connection
Thermal protection will consider starting phase with the line current = current via CT and running phase with line current = 1.73 * current via CT.

If you start your motor using starting reactor or autotransformer, or if you use star-delta start but TesysT is connected in line circuit (not inside motor delta), the motor star-delta parameter must be disabled. The line current is always equal to current via CT.

Switching from step 1 to step 2 is done according to conditions set in threshold and timeout
picture 2

Picture 2 - Configuration example for star delta

In my configuration, switching from star to delta is done if motor current goes below 145%FLC (of course at the beginning of starting the current must go above 145%FLC) or after 5 seconds since start command, whichever condition is fulfilled earlier. 1second is interlock between star-delta switching.

To sum up, in start-delta start, always set FLC current to the value shown on motor plate for delta connection, which is steady current during motor running.
If supply network is 400V, 50Hz the motor plate should look like :
Y / D
690V/ 400V
17A / 30A (example)

FLC to be set to 30A

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.