Issue
User has devices in their system which do have the onboard alarming capability to detect an Over Voltage Condition
Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Environment
Web Applications
Alarm Configuration Tool
Cause
User would like to set up an Over Voltage alarm for multiple devices in their system.
Resolution
Based on the installed PME version please see the videos below which demonstrate how to configure an over voltage alarm template using the Alarm Configuration Tool. It also describes how to apply this template to multiple devices in a system.
PME 8.x
PME 9.0
h