Issue:
Motor current ratings for the ATV680 low harmonic 600 hp and 700 hp drives
Product Line:
ATV680
Environment:
All
Cause:
Motor current ratings not listed in the manual.
Resolution:
The ATV680C40Q4X1 = 600HP 730 amps
The ATV680C50Q4X1 is 700HP 900 amps
The attached document shows the ATV680 being available up to 800KW but you can only get this unit for now up to 700HP normal duty.
Motor current ratings for the ATV680 low harmonic 600 hp and 700 hp drives
Product Line:
ATV680
Environment:
All
Cause:
Motor current ratings not listed in the manual.
Resolution:
The ATV680C40Q4X1 = 600HP 730 amps
The ATV680C50Q4X1 is 700HP 900 amps
The attached document shows the ATV680 being available up to 800KW but you can only get this unit for now up to 700HP normal duty.
Released for:Schneider Electric Saudi Arabia