{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to use the command interface in Modbus in iEM3000 series?
When using command interface in Modbus, the commands must be sent in block, which
means to send all registers at the same time. For the registers marked as reserved, he can set value 0
or random but in one block.
See examples below, for more information about Modbus implementation please refer to iEM3000
series user manual Ref: DOCA0005EN-05

See examples in attachment.

Schneider Electric Saudi Arabia

Attachment(s)
858PRG How to use the command interface in Modbus in iEM3000 series.pdf [262.42 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.