Issue
The meter's front panel status code is displayed in hexadecimal without a full explanation of what the hexadecimal value represents.
Product Line
PM5500 series (PM5560, PM5563)
Environment
Front panel
Resolution
Use the following instructions to decipher the status code. In this example, the status reads "0021 hex".
In this example, Bit 01 and Bit 06 are high.
Therefore, this device appears to be having a clipping issue, and the customer must evaluate the voltage and current inputs to confirm they are within the meter's specification.
Note: an error code of 0011 denotes a calibration failure. In this scenario, the meter should be returned as part of the RMA process.
The meter's front panel status code is displayed in hexadecimal without a full explanation of what the hexadecimal value represents.
Product Line
PM5500 series (PM5560, PM5563)
Environment
Front panel
Resolution
Use the following instructions to decipher the status code. In this example, the status reads "0021 hex".
- Convert the hexadecimal value to binary.
0021 | = | 0000 0010 0001 |
Hex | Decimal |
- Determine which Bits are a "1" or high.
0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 1 |
Bit 11-16 | Bit 10 | Bit 09 | Bit 08 | Bit 07 | Bit 06 | Bit 05 | Bit 04 | Bit 03 | Bit 02 | Bit 01 |
In this example, Bit 01 and Bit 06 are high.
- Apply the Bitmap found in the Modbus Register List at Register 20003.
Bit 01 = Summary ( on if any other bit is on - Maintenance Icon (Wrench) shown on HMI )
Bit 02 = RAM Failure
Bit 03 = NVRAM Failure
Bit 04 = RTC Failure
Bit 05 = Calibration Failure
Bit 06 = Clipping Detected
Bit 07 = Over-Running Energy Pulse Output
Bit 08 = Inp Mtr Diag Rate Exceeded/Backup RAM failure
Bit 09 = Lang File Mismatch
Bit 10 = Lang String Mismatch
Bit 11-16 Not Used
Bit 02 = RAM Failure
Bit 03 = NVRAM Failure
Bit 04 = RTC Failure
Bit 05 = Calibration Failure
Bit 06 = Clipping Detected
Bit 07 = Over-Running Energy Pulse Output
Bit 08 = Inp Mtr Diag Rate Exceeded/Backup RAM failure
Bit 09 = Lang File Mismatch
Bit 10 = Lang String Mismatch
Bit 11-16 Not Used
Therefore, this device appears to be having a clipping issue, and the customer must evaluate the voltage and current inputs to confirm they are within the meter's specification.
Note: an error code of 0011 denotes a calibration failure. In this scenario, the meter should be returned as part of the RMA process.
Released for:Schneider Electric Saudi Arabia