{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Can you create a status object in Vista for a Software Alarm rule in PME?
Issue
A user has created a Software Alarm rule within PME's Web Applications and would like to create a Status object in Vista to display it.

Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022

Environment
Vista / Software Alarms

Cause
How to create a status object in Vista for a Software Alarm rule in PME

Resolution
When an alarm rule is created within Software Alarms a corresponding entry will be created within the Measurement Modules for the sources selected. The screenshot below is from a Communications Loss Alarm.

Screenshot of Vista Module

Schneider Electric Saudi Arabia