Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate and configure the Zero and Full scale value for a PM8000 Analog Input
Issue
Configuring the analog input on a PM8000.

Product Line
PM8000 series

Environment
Meter Configuration

Cause
Unlike other ION devices, the PM8000 analog input is only rated for 4-20mA rather than 0-20mA.

Resolution
Per the ION Reference, the Zero Scale can be calculated as follow:

Zero Scale = FullScale - (FullScale - X)(Af - Ax)/(Af - Aa)

where
Aais the analog hardware output minimum range value.(For the PM8000, Aa is equal to 4 mA.)
Afis the analog hardware output maximum range value.(For the PM8000, Af is equal to 20 mA.)
Axis the analog hardware output minimum value.(For the PM8000, Ax is equal to 4 mA.)
Xis the scaled equivalent of Aa.(This is determined by the device sending the Analog signal.)

The previous equation can be simplified to:

Zero Scale = FullScale - (FullScale - X)*(Af - Ax)/(Af - Aa)
Zero Scale = FullScale - (FullScale - X)*(20 mA - 4mA)/(20 mA - 4mA)
Zero Scale = FullScale - (FullScale - X)
Zero Scale = X

Therefore, the Zero Scale should correspond with the 4mA value.

For example, if a PM8000 meter is monitoring a 0 to 120 kW system and receiving the power information via a 4 - 20 mA analog signal, the PM8000 would need to be configured to have a Zero Scale of 0 and a Full Scale value of 120.

For instructions on programming the Zero Scale and Full Scale values, see attachment below.
Note: From firmware v3.0.0 the PM8000 has an optional Analog I/O (METSEPM890024) version 001.002.000 for 4-20 mA and 0-20 mA.

Schneider Electric Saudi Arabia

Attachment(s)
Zero Scale and Full Scale values instructions.docx [75.93 KB]
How to calculate and configure the Zero and Full scale value for a PM8000 Analog Input
Issue
Configuring the analog input on a PM8000.

Product Line
PM8000 series

Environment
Meter Configuration

Cause
Unlike other ION devices, the PM8000 analog input is only rated for 4-20mA rather than 0-20mA. 

Resolution
Per the ION Reference, the Zero Scale can be calculated as follow:

Zero Scale = FullScale - (FullScale - X)(Af - Ax)/(Af - Aa)

where
Aais the analog hardware output minimum range value.(For the PM8000, Aa is equal to 4 mA.)
Afis the analog hardware output maximum range value.(For the PM8000, Af is equal to 20 mA.)
Axis the analog hardware output minimum value.(For the PM8000, Ax is equal to 4 mA.)
Xis the scaled equivalent of Aa.(This is determined by the device sending the Analog signal.)

The previous equation can be simplified to:

Zero Scale = FullScale - (FullScale - X)*(Af - Ax)/(Af - Aa)
Zero Scale = FullScale - (FullScale - X)*(20 mA - 4mA)/(20 mA - 4mA)
Zero Scale = FullScale - (FullScale - X)
Zero Scale = X

Therefore, the Zero Scale should correspond with the 4mA value.

For example, if a PM8000 meter is monitoring a 0 to 120 kW system and receiving the power information via a 4 - 20 mA analog signal, the PM8000 would need to be configured to have a Zero Scale of 0 and a Full Scale value of 120.

For instructions on programming the Zero Scale and Full Scale values, see attachment below.
Note: From firmware v3.0.0 the PM8000 has an optional Analog I/O (METSEPM890024) version 001.002.000 for 4-20 mA and 0-20 mA.

Schneider Electric Saudi Arabia

Attachment(s)
Zero Scale and Full Scale values instructions.docx [75.93 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.