{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the ATV320 drive to power up with a blank display?
Issue:
The ATV320 drive powers up with a blank display.

Product Line:
ATV320

Environment:
All

Cause:
Power board is inoperative or rectifier circuit is inoperative.

Resolution:
Troubleshooting
Check Line voltage on L1, L2, L3 to make sure it is balanced and correct.
Check the DC bus voltage across PA(+) and PC(-).  It should be (line voltage) x 1.414.  [eg  480V x 1.414 = 678Vdc].  If not, the rectifier is inoperative.
Check the +24Vdc-COM voltage.  If sagging, remove the 24V wiring to see if the external circuitry is shorting out the supply.
Drive will need to be replaced if it is found to be inoperative.

Schneider Electric Saudi Arabia