{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I control ATS48 or ATS22 via modbus as well use remote HMI at the same time?
Remote panel as well as PLC with modbus - both represents modbus masters.
Modbus communication from its principle does not support two masters.
The best solution to share one slave (ATS) between two masters (PLC and HMI) is to use modbus port multiplexer. This device alternates modbus requests, once between ATS and PLC and second time between HMI and ATS and so on.
See attached files for more info about PXP-314MB port multiplexer.

Schneider Electric Saudi Arabia

Attachment(s)
PXP314MB.zip [3.77 MB]