{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are temperature settings required for "T" type thermal protection on Trihal dry type transformers?
The transformer rating plate shows temperature rise class "F", which requires the user to apply setting of the T digital thermometer/controller with a maximum temperatures of:
  • 140°C for "alarm 1" and,
  • 150°C for "alarm 2".

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: