Search FAQs
How do I define a class PX current transformer?
Class PX current transformers are generally being defined in terms of the internal characteristics of current transformer as follows:
It is important to know that the parameters of the above formula are dependent on the actual current transformer characteristics and the protection application requirements.
It is important to know that the parameters of the above formula are dependent on the actual current transformer characteristics and the protection application requirements.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: