Issue
STMSDK COM object initialization error when starting Unity after installing PES
Product Line
Unity
Environment
Windows 10
Resolution
Attempts to start Unity after installing PES returns the message ' Error when initializing programming unit (STMSDK COM object initialization):
Unexpected exception (memory allocation, ...
This error will appear if the 'Visual C++ Redistributable for Visual Studio 2012 Update 4' is corrupted. To resolve the issue, re-install or repair
the 'Visual C++ Redistributable for Visual Studio 2012 Update 4'
The installation files for the 'Visual C++ Redistributable for Visual Studio 2012 Update 4' can be downloaded from:
https://www.microsoft.com/en-us/download/details.aspx?id=30679
Released for:Schneider Electric Saudi Arabia