{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up a logic input for Jog on the ATV312 drives?
Issue:
Jog function on the ATV312 drives.

Product Line:
Altivar Machines, Altivar 312, Altivar 31

Environment:
All

Cause:
set up a jog speed of 10hz.

Resolution:
FUN menu
Jog settings (JoG-)
Jog (JoG) set to Logic input X example LI6
Set jog speed (JGF) 10hz

(you will still need a direction Forward or Reverse on LI1 or LI2)

Schneider Electric Saudi Arabia

Attachment(s)
ATV312_programming_manual_EN_BBV46385_03.pdf [2.84 MB]