{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the recommended lug kit for a Frame Size 6 Process Drive?

Article available in these languages: Spanish

Issue:
Frame Size 6 Process Drive Lug kit part number

Product Line:
Altivar Process Drives (ATV6xx, ATV9xx) Frame Size 6

Environment:
All

Cause:
NA

Resolution:
This applies only to frame size 6, which includes the following drive part numbers:
ATV630D55M3ATV930D55M3C
ATV630D75M3ATV930D75M3C
ATV630C11N4ATV930C11N4C
ATV630C13N4ATV930C13N4C
ATV930C16N4ATV930C16N4C

The part number for the Lug Kit is DZ2FH6. This kit has quantity of 6 lugs. Individual lugs can be ordered with part number DZ2FH1.
This document provides further detail an installation instructions: https://www.se.com/ww/en/download/document/NHA95647/

Schneider Electric Saudi Arabia

Attachment(s)
ATV_Process_size6_IS_LUG_kit_NHA95647_00.pdf [1.28 MB]