{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SFT2841 Setting and Operation Software Overview
Issue
Overview of the SFT2841 software for the SEPAM relay.

Product Line
SFT2841
SEPAM 20
SEPAM 40
SEPAM 80

Resolution
The SFT2841 software is the setting and operating tool for SEPAM series 20, SEPAM series 40 et SEPAM series 80. It may be used in 2 operating modes:
  • unconnected to SEPAM, to prepare parameter and protection settings
  • connected to SEPAM, to download and upload SEPAM parameter and protection settings and have access to all operating functions.
Please see attachment for more information.

Schneider Electric Saudi Arabia

Attachment(s)
SFT2841 setting software.pdf [266.91 KB]