What causes an 00h or 86h error in Vijeo Designer when communicating to a M221 PLC?
The error message is due to the Magelis reading the discrete/analog inputs as %I or %IW from the PLC. You need to move the %I and %IW to %M and %MW in order to read the data from Vijeo Designer.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Vijeo Designer
Modicon M221
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.