There is no option to add an Ethernet option on the non E suffix ATV340 drives. If the Ethernet port on the ATV340.....E fails you can not replace the module its not replaceable. The non E suffix version or Standard ATV340 does support modbus but not Modbus TCP.
Only the E version of the ATV340.....E drive supports Both Modbus TCP and Ethernet IP.
On a side note only the none E suffix version allow the other option cards not the E suffix version.
1:) CANopen
2: )PROFIBUS DP V1
3:) DeviceNet
4:) EtherCAT
5:) ProfiNet
Released for: Schneider Electric Saudi Arabia


Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.