{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212 is configured to communicate via Modbus. How to reset the drive when the drive is showing an error?
If you can communicate with the drive while display shows error, then you can reset the drive fault over modbus using bit 13 of command word.
See attached page from ATV212 manual.
The fault of course must be "resetable". List of all resetable faults can be found in ATV212 programming manual.

Schneider Electric Saudi Arabia

Attachment(s)
Extracted pages from ATV212 Modbus_manual_EN_S1A53844_01.pdf [68.14 KB]