{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Single Phase Reversing NEMA Combination Starter
Issue:
Are there any single phase reversing options for NEMA combination starters?

Product Line:
8502, 8536, 8538, 8539, 8702, 8736, 8739, 8739

Environment:
NEMA Contactors and Starters

Resolution:
There are not any single phase reversing combination starters in the NEMA offering.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.