{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Universal Transfer Switch; Fuse Removal and Manual Circuit Bypass.

Issue:
APC Universal Transfer Switch; Fuse Removal and Manual Circuit Bypass.

Product Line:
APC Universal Transfer Switch
UTS6, UTS6BI, UTS6H & UTS10BI

Environment:
All Models

Cause:
The unit is no longer passing power via one of the UTS electrical circuits.

Resolution:

Safety Precautions: Any work internal to the UTS must be preformed by a licensed electrician. Prior to accessing the Universal Transfer Switch, all power must be secured at the electrical breaker panel, as well as any Generators or UPS which may be attached.

The following video details the process for removal and replacement of the circuit fuses as well as manually bypassing the UTS circuits.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: