{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NetBotz Rack Monitor 250 Modbus Register Map Detail for MM_SENSOR_1_DISCRETE_STATE register/data point
Issue

The NetBotz 250 Modbus Register Map references this FAQ article to further explain the possible responses/ENUM for the following register/data point:
  • MM_SENSOR_1_DISCRETE_STATE

Product Line
  • NetBotz
    • ​NetBotz Rack Monitor 250


Environment
  • All serial numbers
  • All firmware versions
  • Modbus TCP/serial users

Cause

This article will provide additional information and detail for Modbus users.


Resolution

Within the NetBotz 250 Register Map, discrete (state) sensors refer back to MM_SENSOR_1_DISCRETE_STATE as needed to provide what possible responses may exist. Modbus responses of 1 and 0 may refer to different discrete sensor states depending on sensor type. The below information clarifies what is mentioned in the NetBotz 250 Register Map document.

MM_SENSOR_1_DISCRETE_STATE

The following responses are supported for MM_SENSOR_1_DISCRETE_STATE:
  • 0 = Open (Low)
  • 1 = Closed (High)
  • 2 = Not Connected

The above possible responses will also be used by the following supported sensor types for MM_SENSOR_1_DISCRETE_STATE:
  • Smoke (NBES0307) - 0 = No Smoke, 1 = Smoke Detected, 2 = Not Connected
  • Fluid (NBES0301) - 0 = No fluid, 1 = Fluid Detected, 2 = Not Connected
  • Vibration (NBES0306) - 0 = No Vibration, 1 = Vibration Detected, 2 = Not Connected

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: