undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the WSOS V5 Software work on Windows 10?
Issue
Does WSOS V5 software support Windows 10?

Product Line
WSOS

Environment
Reclosers

Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.

This is from page 6 of the release notes of the software

"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.

There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.

The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."



 

Schneider Electric Saudi Arabia

Attachment(s)
WSOS5 - Release note-Version-03.pdf [998.04 KB]
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.