{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Efficiency of the EV Link Chargers?
1) Inside EV Link a mother board with a 24V power supply commanding a contact is installed.
2) Less than 100W of consumption when the CT is closed. We are just a gate between the grid and the car.

So the maximum consumption is 100w (dedicated to 24v power supply, motherboard, contactor and led). Efficiency will be,
If the load is a 3,7kW (16A 1P) efficiency = 97%
If the load is a 22kW (32A 3P) efficiency = 99,5%

But, also consider the Harmonics, Power factor produced by the Car itself which will affect efficiency.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.