undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Rated impulse withstand voltage (Uimp) value for Frequency inverter Altivar Process ATV600, ATV900?
ATV process product datasheet declares under electromagnetic compatibility that it complies Electrical fast transient/burst immunity test level 4 according to IEC 61000-4-4
In this standard, the peak value of the voltage for level 4 is 4kV, see table in attachment. From this reason ATV process must withstand impulse voltage of 4kV.
Conditions for repeated impulse withstand test as well as parameter of the impulse are specified in this standard IEC61000-4-4.

Schneider Electric Saudi Arabia

Attachment(s)
ATVp-testVoltage.jpg [106.68 KB]