{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How can I find the Time Constant of older braking resistors for use with the ATV900 series drives?
Issue:
Time Constant for older braking resistor I want to use with my ATV900.

Product Line:
ATV900 series drives.

Environment:
All models, All serial numbers where a braking resistor is being added.

Cause:
The ATV900 series drives requires a "time constant" setting when using a braking resistor.  This information is not available for older resistors.

Resolution:
It is recommended to use the braking resistors in the ATV900 catalog which have this value listed.  Resistors from older applications may not be compatible with the braking resistor/transistor system of the 900 series drive.  This information will not be available on some older resistors.

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.