Does the TeSys T LTME Expansion Module require the connection of the LV1/LV2/LV3 phases to operate the logic inputs?
No, There is no need to connect main power on L1/L2/L3 on the LTME terminals to operate and use the Logical inputs. The LTME expansion modules are powered by the LTMR controller via a connector cable.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Tesys T
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.