{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the Accuracy Class rating of the CT calculated?
Product
Current Transformers

Environment
Power Monitoring Instrumentation

Cause
Accuracy class is used to classify how accurate current transformers can measure current without error. There are 3 accuracy classes for Schneider Electric current transformers: class 0.5, class 1, and class 3.

Resolution
The accuracy class rating of the CT is based on the Max Power (VA) for the CTs
If the meter (VA) + the cable (VA) is less that Class 0.5 Max VA of the CT, the CT is class 0.5.

For documentation for Schneider Electric CT’s please check FA311758




Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.